Set Higher Standards for Resistors Panasonic

Set Higher Standards for Resistors Theme Image

Resistors are arguably one of the most fundamental electronic components and are key for every single electronic circuit in existence. Some resistors are found as old-fashioned wire-wound parts soldered onto printed circuit boards (PCBs) by hand, while others are integrated into integrated circuits (ICs) directly in the form of polysilicon traces.

In this blog, we will look at the importance of resistors in modern electronic design and how the latest Panasonic range of resistors can help engineers reduce the cost of their products while making them more efficient.

Resistors in History

One of the oldest mass-produced resistors is the carbon composition resistor. It consists of a cylinder made of a carbon/ceramic power mix, which is bonded with a resin, and a pair of metal caps with component legs attached to either end. While these resistors were useful for early electronics (such as amplifiers and radios), they quickly became problematic for a multitude of reasons.

Needless to say, it did not take long for the industry to develop a wide range of resistor types, all with their own advantages and disadvantages. Wire-wound resistors find themselves in power applications in which a standard carbon resistor would vaporize, while some metal film resistors have proven incredibly popular in precision circuitry that requires resistance tolerances of less than 1 percent.

The resistor market today is one that would dazzle even the most experienced engineer—parts coming in all different shapes and sizes, all for use in specific applications. To make matters more complex, technology is evolving, with a rapidly growing interest in Internet of Things (IoT) technologies and solutions that are requiring continuously reduced circuit sizes. And that’s not to mention wearable electronics that require flexible circuits and power circuitry that needs to handle more power in smaller spaces.

A New Standard Line of Resistors from Panasonic

Panasonic not only recognizes the importance of resistors but is releasing a new line of resistors to help engineers produce smaller and more efficient designs. In Panasonic’s new offering, the older line of resistors (the ERJ line) has either been made smaller while handling more or the same amount of power or increased in power dissipation in the same footprint.

Taking a closer look, Panasonic was able to increase the power dissipation of surface mount resistors courtesy of improved trimming technology. You see, standard surface-mount device (SMD) resistors use straight lines in an L shape to trim the resistor to the specified resistance. The problem here is that it winds up creating sharp corners of material which result in “hot-spots”. Despite the rest of the resistor being able to handle more power, it is these hot-spots that cap the maximum power dissipation and also cap the maximum pulse current (Figure 1).

Comparison of Panasonic’s legacy and new resistors' power handling capabilities.

Figure 1: The image compares the power handling capabilities of Panasonic’s legacy resistors and their new standard resistors. (Source: Panasonic)

Panasonic’s new trimming technique uses curved lines from both sides of the resistor. Doing this almost entirely removes the hot-spots because of an overall 64 percent reduction in their power ratio (Figure 2). What’s more, this trimming technology also improves the pulse characteristics, allowing the ERJP series to typically handle double the power in the same case size.

Power ratio comparison of Panasonic’s new and legacy resistors.

Figure 2: Power ratio comparison of Panasonic’s new standard resistors and legacy resistors. (Source: Panasonic)

The use of curved and meandering trims on the new line of resistors has led to smaller parts with greater power handling capabilities. The new design enabled Panasonic to reduce the overall footprint and weight of their resistors. For example, a product using 10,000 1206 standard SMD resistors can use 0805 high-power parts in their place and reduce the total weight by 40g (a 60 percent reduction) and use up to 50 percent less PCB space.

It’s also worth pointing out that Panasonic’s new line of resistors come in several variations to serve many different applications. For example, the ERJUP6 is a 0.5W resistor in a 0805 footprint with anti-sulfur and anti-surge capabilities while the ERJT06 is a 0.25W resistor also in a 0805 footprint but is specialized for anti-pulse applications.

The new line of ERJP resistors have tolerances as low as ±0.5 percent, are available in resistances ranging between 1Ω to 10MΩ, a temperature coefficient of resistance (TCR) of ±100ppm/°C, and a temperature range between -55°C to +155°C.

Implementation Examples of the New Line of Resistors

ERJPA2

The ERJPA2 is a 0402 SMD resistor capable of dissipating 0.2W of power and is a potential drop-in replacement for the older ERJ2 or can be used to replace the ERJ3 or ERJ6 if a smaller pad and higher power dissipation are required.

ERJPA3

The ERJPA3 is a 0603 SMD resistor that is capable of dissipating 0.25W of power and is a potential drop-in replacement for the older ERJ3 or can be used to replace the ERJ6 if a smaller pad and higher power dissipation are required.

ERJP03

The ERJP03 is a 0603 SMD resistor that is capable of dissipating 0.2W of power and is a potential drop-in replacement for the older ERJ3 or can be used to replace the ERJ6 if a smaller pad and higher power dissipation are required.

ERJP06

The ERJP06 is a 0805 SMD resistor capable of dissipating 0.5W of power and is a potential drop-in replacement for the older ERJ6 or can be used to replace the ERJ8 if a smaller pad and higher power dissipation are required.

ERJP08

The ERJP08 is a 1206 SMD resistor capable of dissipating 0.66W of power and is a potential drop-in replacement for the older ERJ8 or can be used to replace the ERJ14 if a smaller pad and higher power dissipation are required.

It can be seen that the new line of resistors not only reduces the size of the resistor for the same power but can also increase power capability. But how do reduced resistor size and higher power dissipation help designers, and what can an engineer expect when using the new Panasonic line of resistors?

The Benefits of Smaller, More Powerful Resistors

Using parts that are smaller and able to handle more power has many advantages, some of which are not entirely obvious at first.

First, resistors such as the ERJP03 not only act as a potential drop-in replacement for the older ERJ3 (i.e., no need for footprint changes on older PCB designs), but they can handle more power and, therefore, can be used to either replace larger resistors or combine multiple small resistors used in parallel to improve power dissipation. The reduction in part count can help to reduce bill of material (BOM) costs and, therefore, the cost of the overall manufacturing process.

Replacing older resistors (e.g., ERJ8) with smaller resistors (e.g., ERJP06) with either the same or greater power dissipation can have a dramatic effect on the overall design of a PCB. The use of smaller components helps to save previous PCB retail space, which drives down the cost of PCBs. The saved space also helps to reduce the overall size of the circuit, which has a number of benefits. For one, smaller circuits often have smaller trace lengths, which can be highly beneficial in environments where EMC may be a concern. Second, smaller circuits are more portable and easier to integrate into tight environments such as wearable electronics. If smaller components are used but the PCB size is kept the same, then the designer has the opportunity to integrate more functionality into their product and, therefore, improve the capabilities of the end product.

Combining the use of smaller and fewer parts also affects the manufacturing aspect. Having fewer components to place in a smaller space allows for more PCBs to fit onto a single panel and reduces the time for pick-and-place machines to populate the PCB. Having fewer solder joints also reduces the number of potential failure points both during manufacture and when in service. The use of fewer solder joints also helps to reduce the time required for automatic optical inspection (AOI) or can allow for more components to be inspected in the same amount of time.

Conclusion

Choosing the right resistor for your design is an important task, and with so many resistors available, it can be truly daunting. Panasonic not only recognizes the importance of resistors but is pushing the boundaries of technology to produce resistors that are smaller and more efficient.

The Set Higher Standards for Resistors blog was written by Panasonic and was first published on na.industrial.panasonic.com.



« Back


Panasonic LogoPanasonic Corporation and its subsidiaries (Panasonic Batteries, Panasonic Electronic Components & Panasonic Industrial Devices) are innovators in consumer electronics and technology products. Guided by a mission to contribute to the progress and development of society and the well-being of people worldwide, Panasonic is a strong proponent of responsible electronics recycling and of reducing the global carbon footprint. Panasonic Corporation was named to the 2008 Global 100's list of the Most Sustainable Corporations in the World.


All Authors

Show More Show More
View Blogs by Date

Archives